Renesas has created a solution for tracking man’s best friend. The Pet Activity Monitor is an example how our specific products can receive signals (barking or movement), provide signal integrity, feed information to the MCU, and process data so it can be displayed or read from a PC application.
The Pet Activity Monitor features a Renesas Synergy™ Platform S3-series MCU, and multiple power/analog components from the product line.
Features Include:
- Detects movements/steps
- Uses MEMS microphone for audio detection
- Low power consumption
- Powered with one rechargeable coin cell battery
- Designed using Renesas Synergy SSP API
- Expandable with the Serial PMOD port