Enter to Win an AE-CLOUD2 Kit

Renesas Synergy AE-CLOUD2 KitThe new Renesas Synergy™ AE-CLOUD2 Kit is a complete hardware and software reference design that allows embedded developers to quickly evaluate cellular connectivity options and build Low Power Wide Area (LPWA) cellular Internet of Things (IoT) applications. The AE-CLOUD2 Kit together with the new Synergy Software Package (SSP), version 1.5.0, simplifies connecting IoT sensor devices to enterprise cloud services using 4G/LTE Cat-M1 and Cat-NB1, with fallback to 2G/EGPRS cellular networks. The kit includes:

  • Synergy S5D9 MCU board
  • Wi-Fi module
  • Cellular Arduino Shield
  • Two (2) USB cables and one (1) Ethernet cable
  • Cellular antenna and GPS antenna

Fill out the form for your chance to win a free AE-CLOUD2 Kit!

Please note that the AE-Cloud 2 kit requires a SIM to activate the cellular connection. The process to acquire and install this SIM depends on the selected telecom regional carrier. For more details, please see our SIM activation process knowledge base article.

This promotion has ended.