On-Demand Webinar
The trend towards digitalization and IoT is progressing rapidly in recent years. As a result, our lives have changed to become more convenient and enriched, but the valuable data and information exchanged are facing security threats.
Implementing autonomous security in each IoT device can counter security threats. With Renesas' RX Security solution, the implementation becomes easier than imagined. Implementing security in the MCU will further strengthen the system security as it is the starting point of the IoT device operation.
Learn about the following information from the webinar:
- Challenges for achieving security
- RX MCU security solution based on the hardware security function
- Partner solution supporting the implementation of security functions using the RX MCU
Presented by:
Michael Sarpa
Renesas Electronics
Michael Sarpa is responsible for product marketing and customer development for Renesas' flagship RX 32-bit MCU product line. Michael's 25+ years of experience working with and supporting embedded developers provides customers and ecosystem partners an excellent resource when developing next-generation platforms.