On‑Demand Webinar
MikroElektronika mikroBUS click boards are plug‑in play solutions designed to revolutionize the way users add new functionality to development boards. The user can push a click board into the innovative new mikroBUS socket and use it with zero hardware configuration. Categories of mikroBUS adapter click boards include wireless connectivity modules, wired communication modules, sensor modules, display modules, interface modules, and miscellaneous modules and accessories.
The TINY Bluetooth LE Click is a Click board™ compatible Bluetooth Low Energy solution featuring the worldwide certified SmartBond DA14531 Bluetooth LE 5.1 Module. This enables a user to quickly develop simple standalone Bluetooth LE applications or to add a BLE data pipe to an MCU. The Bluetooth LE TINY Click is pre‑programmed and supported by an easy‑to‑use SDK from Dialog along with a number of useful software examples including CodeLess™, an AT Command‑based solution requiring little or no code development. It’s also supported by MikroElektronika’s mikroSDK, which includes functions that simplify software development.
During this webinar, we will:
- Highlight mikroBUS and the DA14531 Module - what is it?
- Show how easy it is to work with a mikroBUS accelerometer sensor click board plugged into a DA14531 TINY™ Click board
- Show how to add a Bluetooth LE data pipe to an MCU
- Demonstrate how simple it is to start prototyping using the TINY BLE Click board
Presented by:
Alex Kengen
International Product Marketing Manager
Renesas Electronics
Alex has close to 20 years of experience in the Telecom and Semiconductor industries and has served in a variety of roles ranging from system engineering to marketing and international business development. He is responsible for driving Renesas connectivity leadership and growth in the consumer market.
He earned a Master of Science in Industrial Design and Production Engineering from Delft University of Technology in the Netherlands.