On-Demand Webinar
Renesas, as one of the top-tier semiconductor manufacturers, released its latest power management IC solutions for the emerging 48V architecture in 5G telecom, computing, and beyond. ISL81801 is an 80V bi-directional buck-boost controller, while ISL81802 is a dual output / two-phase sync buck controller with a ton of exciting features. They both have constant current and constant voltage regulation capabilities, making them ideal for applications like battery charging, renewable energy, automotive power, and other wide input or wide output industrial applications.
Presented by:
Zhihong Yu
Staff Product Marketing Manager
Renesas Electronics
Zhihong Yu is a Staff Product Marketing Manager at Renesas Electronics America since 2018, leading the indusrial power product lines of the Industrial and Communications Business Unit. From 2011-2018 he was a Product Marketing Manager at Monolithic Power Systems on ACDC, lighting, sensor, and driver products, and held positions at International Recitifer (now Infineon). He graduated with a BS Degree from Shanghai Jiaotong University, and an MS Degree from Northern Illinois University.