On-Demand Webinar
Most IoT devices are made of the same basic elements. You have sensors to collect analog or real-world data. You then feed this data to a processing unit like a microcontroller or microprocessor to synthesize the data. Finally, you apply power to the entire system via line power or a battery. If it is so simple though, why is the development effort mired in issues like incompatible sensors, lack of development kits, or missing and incomplete software?
The Renesas Quick-Connect IoT system is a revolutionary new modular building block system that simplifies integration of sensors, connectivity, and processing, not only in hardware, but also in software. The hardware modules can be daisy chained, meaning you can easily integrate multiple devices on one platform. The software is integrated directly into Renesas’ most popular development environments like the Flexible Software Package and e² studio. This powerful hardware and software combination will usher in a new era of ease-of-use and development productivity.
In this webinar, you will learn:
- How the Pmod™ type 6A hardware architecture makes it simple to connect to any Renesas development kit
 - How the integrated software reduces integration effort by providing software libraries and simple software APIs
 - How the combined hardware and software solution of the Renesas Quick-Connect system simplifies the transition from prototype to production
 
              
              Brad Rex
Sr Manager, System and Solution Team
Renesas Electronics
              Brad has over 20 years of experience in embedded design and development, covering both hardware and software. Starting with ASIC design and verification, he moved on to directly supporting customer software development as both an Applications and Field Applications Engineer, successfully getting a wide variety of customers ranging from consumer, industrial, and automotive into production. Brad holds an Electrical Engineering degree from the University of Arizona.